Part Number: TLC555
Other Parts Discussed in Thread: TINA-TI
How do you calculate the maximum capacitor capacity that can be used it?
I would like to know if 1Mohm register and 33uF capacitor can be used with 6.5V power supply for 30sec timing.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For the monostable circuit, the capacitor can be back calculated based on timing and resistor requirements from the following formula:
C = t/(1.1*R)
For 1M and 33uF I calculate a pulse width time of 36.3 seconds. I have simulated this in Tina-Ti (attached at the bottom of this post). This works as expected. In order to get more precise you could change the resistor value or do a parallel resistor combination to get the exact value resistor you desire for the design such that the timing is more accurate.

For more in depth information on both the monostable and a-stable modes we have some information here:
Best Regards,
Chris Featherstone