Part Number: LMX2592
I have an application in which I need to ensure phase synchronization to within about 10 degrees between multiple synthesizers over a long period of time (months) with or without power cycling. I would like to know if the LMX2592 is a suitable device for this. If I synchronize and set the relative phase relationship of multiple LMX2592 synthesizers connected to the same frequency reference per the information in the datasheet, will the relative phase relationship between the LMX2592 synthesizers stay fixed over a long period of time? Will the relative phase relationship stay the same, if I power cycle occurs and the synthesizers are re-programmed back to their original settings? I'm concerned that they may drift apart over time or noise on the reference signal might affect the long term synchronization.