Part Number: LMK04832
Hi team,
Customer want to learn the timing requirement of t1,t2,t3,t4,t5 as below picture shown when using lmk04832.
Sync is for clock output synchronization. could you pls help it?

Rayna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04832
Hi team,
Customer want to learn the timing requirement of t1,t2,t3,t4,t5 as below picture shown when using lmk04832.
Sync is for clock output synchronization. could you pls help it?

Rayna
Rayna,
A few thoughts before we provide timings:
Now, if the customer is going to generate pin reset and SYNC regardless:
T1: min time = 0. RESET pin can be pulled up with power if desired.
T2: min time = 1µs. We expect the reset to occur within maybe four or five state machine clock cycles, and the state machine clock within LMK04832 is running at 10MHz ± 30%, so 1µs is a safe bet.
T3: min time = 0. Register configuration can occur immediately after RESET pin goes low. SPI communication is slower than state machine clock.
T4: min time = depends entirely on application settings and time for PLL to lock. The SYNC pulse should not be generated before the PLL locks. In principle the SYNC pulse can be generated at any time as long as there is a clock distribution path signal (e.g. the VCO is up and running). In practice there are some configurations which loopback the SYSREF divider as a feedback divider in zero delay mode, and ideally the divider reset should only occur after the PLL locks (especially if the SYNC is re-timed to the SYSREF divider). If there is no input-to-output phase alignment requirement on LMK04832, min time for T4 = 0 and SYNC event can be handled by pin or by software automatically. If there is an input-to-output phase alignment requirement depending on the SYSREF divider in feedback to one of the PLLs, min time for T4 is however long it takes for the PLL with SYSREF divider feedback to lock.
T5: min time = depends entirely on application settings.
Regards,
Derek Payne