Part Number: LMX2571
Hi Team
Customer wanna using an external VCO to output 455.66MHz. and configure SPI port with 4 wires. The reference frequency is 122.88MHz and the reference frequency is single-ended input, the phase detection frequency is 61.44MHz.
The configuration and register and schematic show as below, but it works abnormal and can't lock. Can you help review if there is any fault?
R60 0x3CA000 R58 0x3A8C00 R53 0x357806 R47 0x2F6000 R46 0x2E001A R42 0x2A021E R41 0x290870 R40 0x28101C R39 0x2711FB R35 0x230C83 R34 0x221000 R33 0x210000 R32 0x200000 R31 0x1F0000 R30 0x1E0000 R29 0x1D0000 R28 0x1C0000 R27 0x1B0000 R26 0x1A0000 R25 0x190000 R24 0x18000E R23 0x170E84 R22 0x168584 R21 0x150101 R20 0x14301B R19 0x1303E8 R18 0x120000 R17 0x110000 R16 0x100000 R15 0x0F0000 R14 0x0E0000 R13 0x0D0000 R12 0x0C0000 R11 0x0B0000 R10 0x0A0000 R9 0x090000 R8 0x0800EE R7 0x070EC4 R6 0x068441 R5 0x050101 R4 0x04000B R3 0x031200 R2 0x0232FE R1 0x017A0F R0 0x000082