Other Parts Discussed in Thread: TIDA-01410, LMK00304
Hi all,
We have an application require two outputs of lmx2594 working at the same frequency and phase for beam steering.I have read your reference design TIDA-01410.But there is something different in our design for some reason.The design diagram is as follow and our application belongs to SYNC category 3 :
For the design,i have some questions:
1.Is there some output skew from the lmk00304?
2.Should the trace length from the lmx00304 to two lmx2594 be equal?
3.Is it right for ocsin should be lower than 100M for SYNC category 3?
In short, can the above design realize the synchronous output of two lmx2594?
BR.
hips