Part Number: LMK04828
Hi,
I‘m very curious about
1. How the input SYNC impact SYSREF?
2. why the figure2 is different form figure1 about the flow direction of continue 5MHz SYSREF ?
As below figure1 shown, 5MHz SYSREF frequency is independent with SYNC event fully through SYSREF_MUX, that mean only one could be selected between continue 5MHz SYSREF and SYNC(Normal/re-clocked/pin pulse) as source into SYSREF distribution path directly.
Thanks in advance
Figure1. continue 5MHz SYSREF is input into SYSREF_MUX

Figure 2 continue 5MHz SYSREF is input into SYSREF distribution path directly, why