This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX series synthesizer recommendation

Other Parts Discussed in Thread: LMX2820

Dear forum members 

we are looking to purchase two TI RF Synthesizer With Phase Synchronization.

They should operate in two frequency regimes:

  1.  533.34MHz to 1033.34MHz
  2. 6034.69MHz to 5801.34MHz

Each range 1&2 would be serviced by one LMX. It would be important to maintain a sinusoidal output at all times (so basically not using the divider function to generate the frequency).

Can somebody recommend possible candidates from the TI synthesizer range for this task?

Thank you Nikolaus