Other Parts Discussed in Thread: LMK04832-SP, LMX2694-SEP
Team,
Regarding the LMX2615-SP, LMX2694-SEP, and LMK04832-SP, a term that I have heard in the past was called back driving but that may be an incorrect terminology for my question.
The above mentioned devices use an external clock input. When it comes to space applications it always appears that development is hyper-sensitive to reliability. Should there be concern for a device being powered down with a clock present at its input.
I will be the one providing the clocks to these devices so that is why I am asking the question if I need to make sure that the clock is disabled or terminated so this does not occur.
Thank you.