Other Parts Discussed in Thread: CDCM6208
I want to create a multiplying wave that changes following a reference signal with a fluctuating frequency.
I want to synchronize the reference signal at 1.7MHz and change it within the range of ± 2%.
As a result of testing using the evaluation module (CDCE62005EVM), synchronization was lost about 50Hz before.
Of course, Synchronize when set directly to the maximum and minimum frequencies.
The frequency change is slow enough.
I don't know the cause, so I'd like some advice.
------test date---------
Refarence Frequency :1.7MHz (1.666~1.734MHz)
Reference Divider :1/1
1.602-1.721 :locked
Outside it :unlocked
Output Frequency :163.2MHz(159.936~166.464MHz) :Ref*96
Output Divider :1/4
VCO Frequency: 1.9584GHz (1.919232~1.997568GHz)
Prescaler :1/3
Feedback Divider:1/384
VCO1 used