Part Number: LMX2572
Two questions on manual ramping:
1) Is there a minimum pulse width required for a RampClk edge to be triggered? I know there's a maximum frequency of RampClk of 250KHz (8.1.7.1), and I'm assuming a non-50% duty cycle is okay. So, if I generate a 10ns pulse on RampClk, will it be detected?
2) When manually ramping, does PLL_N automatically roll to the next value when PLL_NUM exceeds PLL_DEN? So, if I start the PLL_N at 50, and PLL_NUM to 0. Can I ramp only until I've maxed out PLL_NUM? Or will it automatically roll PLL_N to 51 and continue adding to PLL_NUM?
Thanks!