Part Number: CDCLVP111
Other Parts Discussed in Thread: LMK01801
I need to make 8x (and 4x and 2x) low skew copies of a 2.5GHz clock. The hard part is that I need between 0.9V and 1.8V of differential swing at 2.5G into 100 ohms (95-110 Ohms) across the pair. I’m sourcing the 2.5GHz clock from a LMK04832NKDT. The LMK04832NKDT was not capable of driving the signal at 2.5GHz. Deterministic skew is fine because I can get rid of it in the PCB.
It doesn't look like the CDCLVP111 can provide that level- please confirm. Are there any other alternatives we can offer?