Part Number: LMK03318
Other Parts Discussed in Thread: TMS320C6678,
Hello,
We are doing some Hyperlynx simulations for the LMK03318 output clocks driving the TMS320C6678 DSP. For the LMK03318 we are using it in Hard-mode with ROM Option 45 (LVPECL outputs). We see from the E2E questions that the DSP IBIS model did not include the termination resistors, so we added those. But we are uncertain as to if the IBIS model for the LMK03318 includes the source output terminations?
Please refer to page 46 of the LMK03318 datasheet for the reference to "No source termination is needed since the on-chip termination is automatically enabled when selecting AC-LVDS, AC-CML, or AC-LVPECL". Are these source terminations a default for the IBIS model, or do we need to make some settings or customization to the model?
The attached spreadsheet has 3 tabs for the 3 clock outputs we are using.
Regards,
Larry