Part Number: CDCE925
Other Parts Discussed in Thread: CLOCKPRO
Dears:
KMM customers need support for the following problems when debugging CDCE925. Could you provide them? Thank you!
Question:
When the customer uses the ClockPro GUI to configure VCXO functionality, the output does not vary with the Vctrl voltage.
Requirements:
24Mhz input, output three frequencies: 12.288m, 3.072m, 0.048m, VCXO mode, the output frequency can be offset with the Vctrl voltage change.
Required support:
Configure the parameters in ClockPro GUI and send the configuration file to the customer for comparison.Or provide a file that is configured to adjust the output with Vctrl.
.