Part Number: LMX2594
Other Parts Discussed in Thread: LMK61PD0A2
Hi Expert,
My customer is evaluating LMX2594EVM.
When They checked the Phase Noise of 8GHz output when the Ref Clock input to the PLL was used with the LMK61PD0A2 set to 100MHz,
The data sheet Figure 53 shows -110dBc / Hz at 10kHz, but the actual measurement is -105dBc / Hz, which is about 5dB worse.
Is it possible to obtain performance of about -110dBc / Hz even when the Ref Clock is LMK61PD0A2?
Ref Clock is a modified EVM and is input differentially.
Loop filters are the default values.
evaluation results
TICS pro setting

Thanks
Muk