Other Parts Discussed in Thread: LMX2594
Hello,
1. For LMX2594 EVM board Schematic, R32 =100 Ohm register is DNP, where for LMX2615 EVM board schematic, R32=100 connected. if i have to use one input RF pin in place of two then what should we have to do?
should we used R32 register or not?
2. what is the line current for VCCBUF, VCCDIG, VCCCP, VCCMASH, VCCVCO2, VCCVCO?
3. What happened if we operate LMX2594 below 3.15 Volt or above 3.45 Volt.