Dear Ladies and Gentlemen
We are using the LMX2571 quite new and we like to have a 6 kSymb/s FSK modulation that is spectrum optimized and high dynamic range.
Do you have good suggestions of does and don't does, to have a very pure TX-signal? Currently we represent the 2-FSK levels with 8 discrete frequency shifts and approximate the low slew rate by the eight discrete steps, but maybe there is a better way to realize the modulation.
We are looking forward to your further suggestions, the application note SNAA309–May 2017 is already known to us.
So to go over I2S seems to be one solution. My question is, would it be also possible to use the PIN mode with the correct designed loop filter, allowing to have the pulse shaping done by the loop filter?
I'm looking forward to your feedback, many thanks in advance.
Thanks and best regards,
Hanspeter