Part Number: LMK00308
Other Parts Discussed in Thread: LMK00304,
Figure 34 in the datasheet shows how to AC couple the LVDS output when used with a device with internal termination resistors. The issue with this is that the LVDS signal is attenuated by the double termination. I noticed in another e2e post on the LMK00304 that a minimum DC termination of 1K ohms was needed to ensure startup of the LVDS driver. Can the 100 ohm near end DC termination resistor in figure 34 be increased to 1K ohms on the LMK00308 when AC coupling the output to reduce the overall attenuation from the double termination?

Thanks for your help,
Mark Dahlman