Other Parts Discussed in Thread: LMK05028
Kia-san,
Please advise on my questions bellow.
Q1. There are two check marks in Validation timer box (left and right of IN0) on TICSPRO GUI,
how they affect to the results?
Q2. There is Trefvalid parameter (.01s to 12.8 s) , how does it influence to the results.
Q3. When the reference frequency is as low as 67 kHz, without turning of the validation timer
(instead of Frequency Detect threshold check box) DPLL did not locked.
Why this occurs?
How much the frequency is classified as Low frequency?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
The .tcs files you provided me did not work.
The LEDs for Status 0 and Status 1 kept on, and the output clock moved against the reference clock
despite of issuing Soft-Reset.
However, when I tried turning off the Validation timer check box, the LEDs for Status 0 and Status 1 turned off, and
output clock stayed against the reference clock
This case, despite of turning on the Frequency detect threshold check box, the DPPL got locked.
I am not fully confident that this action is appropriate and robust workaround for the No Lock issue,
and want to know more about the reference validity check mechanism.
Are there any document which describes the detail mechanism of the reference validity check?
Mita