This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: 2.5V LVCMOS input to PRIREF_P and SECREF_P

Part Number: LMK03318


Hello team,

The customer has simple questions.

Can we input LVCMOS signal from 2.5V LVCMOS driver to PRIREF_P and SECREF_P?

I think that it is no problem because VIL and VIH of PRIREF_P and SECREF_P is meet with 2.5V LVCMOS driver. Is it correct?
The customer is concern because 3.3V LVCMOS driver is used as the recommended circuit in Figure 46 and Figure 47.



Your advice is appreciated.

Best Regards,
Akihisa Tamazaki