This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: Dynamic Digital Delay example

Part Number: LMK04832

We are trying to use LMK04832 Dynamic Digital Delay.
The example in data sheet is used as reference, but I would like to check following.

(In datasheet p34 :8.3.4.3 Single and Multiple Dynamic Digital Delay Example )

Assuming the device already has the following initial configurations:
•VCO frequency: 2949.12 MHz
•CLKout0 = 368.64 MHz, DCLK0_1_DIV = 8
•CLKout2 = 368.64 MHz, DCLK2_3_DIV = 8
The following steps illustrate the example above:
1. Set DCLK2_3_DDLY = 4. First part of delay for CLKout2

Why should DCLK2_3_DDLY be set to 4?

We use 0-Delay mode, is it correct to understand that the CLKout used for feedback cannot be delayed?

Regards,

Sato