Part Number: LMX2571EVM
Other Parts Discussed in Thread: USB2ANY
Hi Team
Let me ask you two questions.
1:
I am using burst mode to continuously change the value of register R33 using TICS pro. is it possible to change the speed of register data transmission in burst mode?
2:
Using equation (4) from the LMX2571datasheet, I obtained the register value that would result in a frequency deviation of 5 kHz and input it to R33. However, the actual frequency deviation from the carrier wave, which was checked using a spectrum analyzer, was approximately 10.5 kHz. We also created the register value representing the negative frequency deviation using equation (6), but the output frequency did not change from the carrier frequency when this value was input to register R33. Why is this happening? The conditions are described below.
fDEV = 5000 [Hz]
DEN = 2^24
fPD = 80 [MHz]
CHDIV1 = 5
CHDIV2 = 2
Prescaler = 2
Input register value (+5kHz deviation) = 147Bh
Input register value (-5kHz deviation) = EB85h
Thank you for your answers.
Best regards,
Nakanishi