Part Number: CDCE706
Hi team,
Could you share the default Reg dump of CDCE706? The datasheet only says non-Reserved bits info.
My customer is facing abnormal heating of CDCE706 and frequency is also strange against settings so I want to be back it to default by the initial Reg setting.
Also, I want to check Revision Code as well. The datasheet says "01h" should be written for Byte 0 but generated setting by TI Clock pro tool shows "11h" for Byte 0.
Which should be correct for now?
Regards,
Takashi Onawa