Part Number: LMK04821
Hello everyone!
I hope this question isn't too simplistic.
I've been looking through the 0482x device family for a JESD204B clock tree design. The 4821, the only device that supports VCO1 division, seems to come up in searches with a max output frequency of 2GHz. However, looking through the datasheet, I can't find the parameter that prevents it from outputting its full 3GHz rate, on par with the 4828.
What am I missing?