Other Parts Discussed in Thread: CDCE62002
Hi,
I have the CDCE62002 EVM - but the computer cannnot find the corrct driver.
I point it to the Driver section of the installation of the installed GUI software- but it fails to find the correct driver.
I get the following :
Description:
Windows detected a new device attached to your computer, but could not find the driver software it needs to make the device usable. Each device manufacturer typically includes driver software of a CD that comes with the device, or as a download from its website. The hardware ID of your device is USB\VID_0451&PID_1E03&REV_0100.
Problem signature:
Problem Event Name: PnPDriverNotFound
Architecture: x64
Hardware Id: USB\VID_0451&PID_1E03&REV_0100
OS Version: 6.0.6002.2.2.0.256.1
Locale ID: 2057
I have copied manualll the CDCE62002.sys file into the system32 directory as the installation did not completed this aspect.
I examined the driver details from Device Manager and there are two entries - the one as above with and without the &REV_0100.
Anyone any ideas how to resolve this ?. Thanks.
Regards,
Richard.