Other Parts Discussed in Thread: CDCE62002
Hi,
I have the evaluation module for the CDCE62002.
For the default start up conditions - 25MHz at the Primary input, the PLL is in lock.
- Can i change the input frequency in the GUI at the Primary input to test if the combination of dividers and other settings will Lock the PLL without having to connect a signal generator to the Primary input SMA ?
I am attempting to use the EVM as a test to ensure that the parameters i have calculated are correct. When i change the input frequency and parameter settings, the PLL does not lock although i meet all the criteria as per the datasheet for parameter settings and boundaries. Hence this question.
Thanks and regards,
Richard.