Part Number: TLC555
Other Parts Discussed in Thread: NE555, , OPA172, OPA197
Hi All,
we are designing a triggered ramp generator, when we have trigger impulse we should generate a ramp from 400mV to 8V with adjustable ramp time.
i will need a potentiometer to adjust the time of the ramp from 1ms to 100ms ( user selectable via potentiometer). eg i set to 10ms, meaning the ramp must go from 400mV to 8V in 10ms.
1) I would like to use NE555 or TLC555 , which one do you suggest to use ?
2) The 555 should operate in monostable operation like on Figure 9 in DS but i want to replace the Ra resistor with a adjustable current source to get a linear ramp on the capacitor.
do you maybe have a simple implementation on how to do this with 555 timer?
and then i will need to buffer the voltage from capacitor to adjust the levels tp 400mV and 8V and to use this signal to drive an actuator.
Br,
D.