Part Number: LMX1204
Hi, I have a strange behavior on my lmx1204. The problem is that then I configure the component as multiplier on R25 and then multiplication factor in R26. Then I read back the registers, the values has changed. The returned value of CLK_MUX is 0x4 (Not a valid value according to the datasheet) and CLK_DIV is has the value of 0x0. I have verified that the SPI communication and the driver is working, so there is not problem there. What parameter I’m missing to get this strange behavior ?
Example of log:
WritingR25(0x67FF)
WritingR26(0x41)
ReadingR25(0x8277)
ReadingR26(0x4940)
Best regards,
Jonas