Part Number: LMK04208
Hi,
In the datasheet of the LMK04208 for NC pin the descriptions says "No Connection. These pins must be left floating." Could you confirm if these pins are internally connected or not?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04208
Hi,
In the datasheet of the LMK04208 for NC pin the descriptions says "No Connection. These pins must be left floating." Could you confirm if these pins are internally connected or not?
Thanks
Hi Mathieu,
I'll check from design side and will get back to you soon.
Thanks!
Regards,
Ajeet Pal
Hi Mathieu,
Most of the “N/C” pins do not have internal connections except a few of them do have internal connections..
For proper operation, you should leave all “N/C” pins floating to preventing potential problems.
Do not connect anything to the N/C pins.
Thanks!
Regards,
Ajeet Pal
Hi,
As I said, I want to avoid floating metal that's why I want to connect these pins (internally or externally to GND or with pull-down).
Can I connect a 1Meg pull down to GND on the N/C pins with internal connections?
Thanks
Mathieu