This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK61E2: Difference between LMK61E2-I5SIAR and LMK61E2-I1SIAR

Part Number: LMK61E2


Hi,

Good Day. What is the difference between LMK61E2-I5SIAR and LMK61E2-I1SIAR? Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hello Ray, 

    The difference between the two OPNs is their default configuration differ along with their default frequencies. For the I5, the default frequency and format is 103 MHz HCSL with an 8 pin 7.0 mm x 5.00 mm package size, where as the I1 contains a 100 MHz HCSL default frequency the same package size.

    Thank you,

    Alexandria