Part Number: CDCE6214
Other Parts Discussed in Thread: CDCE937
Hi
could you help suggest products to replace CY22393
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
I will get back to you tomorrow.
Regards,
Jennifer
Hi Gareth,
The CDCE937 can replace CY22393. Please see a quick comparison table:
| CDCE937 | CY22393 | |
| # of PLLs | 3 | 3 |
| # of outputs | 7 | 6 |
| Output Supply | 2.5 V or 3.3 V | 3.3 V |
| Max output frequency | 230 MHz | 200 MHz |
| Peak-to-peak period jitter | 120 ps (typ) | 400 ps (typ) |
| Package | 20-TSSOP | 16-TSSOP |
| Body Size | 6.5 mm x 4.4 mm | 5.0 mm x 4.4 mm |
Regards,
Jennifer