Other Parts Discussed in Thread: TIDA-01454, LMK5C33216, PCM1864,
Hello,
I would like to have an array of 9 TIDA-01454 Circular Microphone Matrix sample at the same time, but I am not really keen on clocks. So I want to know if this LMK05028EVM is what I am looking for, maybe another product would be better for my project.
In the project it is really important for all the matrix in the array to sample exactly at the same time, so in order to achieve this, clocks must be synchronized between them. But for this I face at least 2 problems:
1. There are 9 CMBs, is it possible to distribute the same clock to 9 devices?
2. The CMBs, will be at a distance up to 5 metres from each other, so this might be a problem when it comes to clock times, attenuation and reflections. So what kind of connection should I use taking in account that the CMB works with Dupont wires?
Thanks,
Mikel