Part Number: LMK05028
Hi,
I would like to ask you a question about the parameter meaning of "DPLL Phase Lock Detectors".
Please tell me the meaning of following parameter set value.
- Lock Threshold
I am currently using the value "31" that changed when I ran MATLAB.
- Unlock Threshold
I am currently using the value "39" that changed when I ran MATLAB.
- Lock LPF Coefficient
I am currently using the value "0" that changed when I ran MATLAB.
- Tph-lock
The time changes depending on the Lock Threshold, but please tell me the details of this.
When Lock Threshold is 31, then 0.1034nSec.
- Tph-unlk
The time also changes depending on the Unlock Threshold, but please tell me the details of this.
When Unlock Threshold is 39, then 26.47nSec.
※ REF TDC Rate[Hz] = 994,646.990740741[Hz]
Thank you for your support.
Takumi