Part Number: LMK03328
Other Parts Discussed in Thread: LMK03318
Hi,
I am using LKMK03328 for clock source.
I need 3-125MHz LVDS
2- 156.25MHz CML
2-25MHz CML
1-100MHz CML clocks for my chips. I need hardware control Mode solution for this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Manish,
LMK03318 is another option if you don't have the need for a second PLL. Both devices have EEPROM that can be programmed.
For programming the device, refer to section 10.5 of datasheet. 
Regards,
Vicente
| Output | Frequency | Type |
| OUT0 | 25 MHz | CML |
| OUT1 | 156.25 MHz | CML |
| OUT2 | 156.25 MHz | CML |
| OUT3 | 100 MHz | CML |
| OUT4 | 125 MHz | LVDS |
| OUT5 | 125 MHz | LVDS |
| OUT6 | 125 MHz | LVDS |
| OUT7 | 25 MHz | LVDS |
Can I achieve above configuration with Hardware Control.
Or I will get only configuration that comes with Defaut EEPROM Image.
Hi Manish,
You can have these frequencies in the desired formats but they would be at different Outputs, not the ones you listed. It would be as follows:
You will not be able to achieve the above configuration with HW CNTRL. You will have to program the device.
Regards,
Vicente