Hi,
I am using the CDCE62002 to produce clock signals for an Audio DAC - and i am now implementing the clock circuit on a daughter board to ensure that if the CDCE62002 fails to be soldered correctly, that the entire DAC board is affected.
I have two PCM1792A's in the new design - one for each channel. i am planning to you SMA connectors from the clock daughter board to the PCM1792A IC's, and thus require two clock outputs. Being a purist, i did not want to clock the PCM1792A IC's with alternate phase clocks from the CDCE62002 output (the other output is clocking the SRC4392).
Hence - i want to use a clock buffer to utilise the positive clock 0 output to send to both PCM1792A IC's.
Which is the preferred clock buffer that does not degrade the low clock jitter of the CDCE62002 ?. Thanks. (CMOS ACT logic ???)
Another related question - i wish to convert the TOSLink output which is a single ended signal to a differential signal which will eventually be connected to the SRC4392 Sample Rate Converter. The length of PCB track will be up to 30cm long - hence the reason for buffering and differential conversion.
Can anyone again suggest a suitable buffer - will standard ACT CMOS logic be acceptable ?.
Thanks and regards,
Richard.