Hi experts,
My customer will use LMC555 with 50% Duty Cycle Oscillator (in the section of 9.6) and the LMC555 will control an LED connected to LMC555's Output terminal. They are planning to make the LED light up when the RESET pin is L and blink when the RESET pin is H. Could you please answer the following questions about how to handle the RESET pin in this case?
Questions about Reset pin
(1) If Reset is kept L all the time after the power is turned on, will the Output be L?
(2) Or is it necessary to set Reset to H when the power is turned on and then change Reset to L?
(3) If Reset is changed from L to H, will the Output operate as an Oscillator?
Question about current output
(4) Does the Current Output Max 100 mA in "6.1 Absolute Maximum Ratings" also apply when sinking current?
Thank you for your help.
Best Regards,
Taito Takemura