This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: I2C Slave Addresses in Register Default Mode

Part Number: LMK03318

Hi

We are using Page Select pins of LMK03318 in Register Default Mode.

When GPIO1=LO, we cannot communicate with the slave address set to 0x50, but we can communicate with the slave address set to 0x54.

Similarly, when GPIO1 = MID, we cannot communicate when the slave address is set to 0x51, but we can communicate when the slave address is set to 0x55.

From this, we assume that the I2C slave address in the case of Register Default Mode is 10101xx, is this correct?

Best Regards,

Hirabayashi