Part Number: CDCE925
Other Parts Discussed in Thread: CDCE937
Hello,
The cdce925 datasheet mentions two "variant" of this device:
CDCEx925: 2-PLL, 5 Outputs
CDCEx925: 3-PLL, 7 Outputs
Later in the datasheet in the table 5 "Slave Receiver Address (7 Bits)" the CDCEx925 device may have a different i2c address:
0x64 for the 2-PLL, 5 outputs
0x6D for the 3-PLL, 7 outputs
But the datasheet is only about the "2-PLL, 5 outputs" variant.
Furthermore there is not device part number for the "3-PLL, 7 Outputs" variant.
Is the CDCEx925 with 3-PLL, 7 Outputs really exist?
If no, the table 5 is actually confusing (error prone) since it is easy to pick the wrong i2c address.
https://www.ti.com/lit/ds/symlink/cdce925.pdf
Best regards,
Romain