Part Number: LMX2571
Other Parts Discussed in Thread: ADC3669, , LMX2572, LMK03318
Hi,
I have a TI ADC(ADC3669 not yet released) which requires clock source of jitter <100fs, one of the App engineer of TI has suggested me to use LMX2571
Kindly help in configuring the LMX2571 device for output of clock frequency of 500MHz
I have two such ADCs, can i use a single LMX2571 for dual 500MHz output simultaneously ?
if LMX2571 is not suitable kindly suggest a PLL based clock source to server the purpose