Part Number: SE555
Hello,
Output pulse duration of SE555's mono-stable operation is estimated as tW = 1.1 × R × C. I'd like to ask how much the constant "1.1" in this equation can change over temperatures.
I guess this equation is derived from tW = -RC ln(1 - VTHRES/VCC), where the VTHRES/VCC is typically 2/3 in the SE555, and the "1.1" comes from -ln(1 - 2/3) = 1.0986 . The SE555 has the Min and Max specs of this THRES voltage level, VTHRES, in its data sheet, however, they are only at TA = 25 °C.
Best regards,
Shinichi Yokota