Part Number: CDCM61001
Dear Sir/Madam,
We would like to use Clock Multiplier Part # CDCM61001 in our USB4 IP Core Development Board.
We would like to have below information to proceed further.
- This Part is taking CMOS input so can we give LVCMOS input clock to it ? We are planning to use this LCMOS Clock output OCXO P/N# DOCAT020V-050.0M for CDCM61001.
- What is Phase Jitter Specification in terms of pSec when we are utilizing 100MHz or 125MHz LVDS Clock Output ?
- Is part under production or under End of Life stage ? Because we have checked that it has very limited stock worldwide ?
- What is Part Life Cycle ? 5 years ? 10 years ?
- What will be the lead time if we will order 100 pcs in that condition ?
Your earliest response will help us lot.