This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832-SP: CLKin input applicatoin

Guru 10920 points
Part Number: LMK04832-SP

Hello,

My customer is considering using the LMK04832-SP for a satellite project.

Here is the CLKin specifications in the datasheet.

Is it possible to use the following clock source as clkin input of the LMK04832-SP without a clock buffer like the diagram above in communication payload on satellite?

    - Single-ended sinewave 10MHz (0dBm, 633mVpp)

    - Sinewave’s slew rate spec = approx. 0.02V/ns

    - Sinewave has atomic clock accuracy, coming in from the outside

Are there any expected problems such as degradation of phase noise performance?

Thank you.

JH