This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214: Questions about the Package Dimensions

Part Number: CDCE6214

The RGE package used by the CDCE6214 appears to have these "corners" on the bottom (A1 ~ A4)

[1]
These anchor pins do not require an electrical connection, but may be connected to GND for better board-level reliability, right?

[2]
I can see the A1~A4 pins are 0.25mm away from the edge of the nearest pin in the x-direction.
But is this also 0.25mm from the edge of the nearest pin in the y-direction?

Regards,
Darren