Other Parts Discussed in Thread: CDCI6214
I understand the CDCE6214 (CDCI6214) both support 4x 100MHz HCSL outputs by default.
Q1:
From Fig. 29 in the datasheet, it looks like the only requirement to load page 0 defaults and get this output without programming, is to pull pin23 LOW, right?
Pins 11/12/19/20 become the output enables, and pin 8 toggles RESET, right?
Q2:
The startup process looks like this, right?
1) Pull pin23 LOW on the PCB
2) Supply power to VDDVCO; keep RESETN LOW until VDD reaches 95% of final value
3) After RESETN voltage rises above 0.8 × VDDREF, device is released from RESET and depending on the OEx pin level, outputs 100MHz HCSL on Y1~Y4.
Q3:
I understand a 25-MHz LVCMOS clock can be input to XOUT(pin1) instead of a crystal.
Should pin2 be connected to GND or left floating? CDCEx datasheet mentions connecting to GND, but CDCIx has no comment on this.
Q4:
pin4 (REFSEL) needs to be set LOW to use pin1 as the LVCMOS clock input (25MHz), right?
Q5:
"Typical Applications" figure in both datasheets show pin23(EEPROMSEL) and pin4(REFSEL) being pulled LOW through 4.7k resistors.
Why this value? I understand internal to these pins there are 50k PU/PD resistors; so couldn't you just tie them to GND? Any reason this was not the described use-case?
Q6.1:
Regarding Enabling/Disabling the outputs.
It looks like there is an internal 50k PU resistor on OEx pins, so if the pins are left floating, the channels are automatically enabled, right?
Q6.2:
If you wanted to disable any of the outputs, you need to pull the corresponding OEx pin LOW, right?