I've been using the CDCV304 in many application as a high speed clock buffer/fannout. However, in this new application, I wonder if I am doing something I should not be with this part. I'm AC coupling (DC block) a high speed CMOS signal (0 to 3V) and feeding it into the clock input of the CDCV304. Therefore my signal is now swinging -1.5V to +1.5V going into CDCV304 input. It seems to be working okay like this but the datasheet says on page 5 that VIH(min) is 0.5VDD (1.65V for me). Is there an internal DC bias that would bias the signal up again?