Dear, Support Team.
Our customer uses the input clock of CDCI6214 with LVCMOS.
When the input clock is LVCMOS, are the FB_N and REFP/N input pins open?
Best Regards,
Hiroaki Yuyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear, Support Team.
Our customer uses the input clock of CDCI6214 with LVCMOS.
When the input clock is LVCMOS, are the FB_N and REFP/N input pins open?
Best Regards,
Hiroaki Yuyama
Hi Hiroaki,
When using an LVCMOS crystal input on the CDCI6214, only the XOUT/FB_P pin is used and the FB_N and REFP\N pins can be left floating. I've attached a recommended schematic for reference. If you are using a non-crystal LVCMOS source, then REFP can be used instead. Also, note that bit 15 of the INPUT0 register will need to be set to 0 to enable LVCMOS inputs.
Regards,
Connor
Hi, Connor-san,
Thank you for your kind reply.
I was able to understand the LVCMOS input pin states and register settings.
Best Regards,
Hiroaki Yuyama