Can each pair of differential outputs of LMX2820 be used as two single-ended outputs? If so, the output power shares the OUTX_PWR setting except that the phase is 180° out of phase?
Also, if two pairs of differential outputs are used as 4 single-ended outputs, what is the approximate power consumption of the chip?
Thanks!