Is there a rule of thumb as to when to use 50 ohm resistor pull-ups vs 68nH + 20 ohms for CML outputs? Based on what I see in the data sheet, it looks like 50 ohms works best at lower frequencies and 68nH =20 Ohms enables higher amplitude output at higher frequencies, but I'm not clear on what frequency ranges would be recommended for each termination method.
A second related question - when selecting CML format, it looks like the frequency divider must be bypassed on the even number clock outputs. TICSPro doesn't appear to give a warning about this when configuring the output clocks. I just want to verify that even number clock outputs cannot use the clock divider when CML output format is desired.