Other Parts Discussed in Thread: LMK04828
Hello E2E team,
I am planning to use the PLL Synthesizer LMX2594 with reference clock from LMK04828B for generating output frequency of 5GHz and 10GHz which is the sampling clock to Data Converter ICs.
Reference clock to LMK04828B PLL is 100MHz from OCXO O-CDFE028EW-P-R-10MHz/100MHz.
I have a very low phase noise requirement at 10Hz Frequency offset for this application.
But in datasheet everywhere i saw the Phase noise plot starting from 100Hz frequency offset.
Can you provide the Phase noise performance data with 10Hz frequency offset at output frequency of 5GHz and 10GHz.?
Please use any low phase noise reference clock for measurement and share the setup details.
Thanks in advance,
Sakthi