Part Number: CDCE937
Other Parts Discussed in Thread: CDCEL9XXPROGEVM,
Hello,
I've just used the CDCEL9XXPROGEVM board to program a CDCE937 clock generator. I'd like to verify it successfully generates the expected clock outputs and its overall performance but I can't seem to be able to do it with the programming board (for instance, there Xin/CLK pin is floating).
On the CDCEL9XXPROGEVM page it's mentioned that 'There is an another EVM available for the purpose of performance measurements and evaluation with part number called CDCE(L)9xxPERF-EVM as Performance Evaluation Module for each of the individual devices'. I can find the performance evaluation boards for all other devices but not for the CDCE937.
Is there a CDCE937PERF-EVM module? Otherwise, how do suggest evaluating the CDCE937 performance?
Thanks!