Hi,
I plan to use CDCM7005 to distribute a 400 MHz clock to several boards. The boards need to be in synch, meaning that not only the input frequency must be the same, but the clocks must also start at the same time. If I initialize the control registers, and then release the /RESET-bit in the control register, will all the outputs start synchronously if they are programmed the same way? Are the clock pulses valid already just after releasing the /RESET-bit (not any glitches/bursts in the start-up)? To summarize, I need to ensure that all the target boards receive the same amount of clock pulses.
This would be a nice way to sync the boards without a separate sync signal.
Br, Karppa